Create Express Stored Display

Once you've completed the configuration in ArcCatalog, open ArcMap and create a stored display that contains the design feature classes (DFCs). This stored display should contain regular features as well as the DFCs that the Express designer will need.

You may want to edit the symbology for the DFCs as well.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?