Reject Session

Changes the session’s status to In Progress and allows the user to assign it to another user.

Enabled

  • MMSessionManager must be the current extension.

  • The selected node is a session.

  • The session must be editable.

  • If the session is open in ArcMap, the user must be editing.

Execute

  1. Prompts the user to select a new user.

  2. Attempts to transfer ownership.

  3. Tells the builder that the user has changed so it can update the tree if necessary.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?