Session Manager Subtasks

Below is a list of the subtasks available for use with Session Manager, the criteria necessary for them to be enabled, and the steps that are performed when they are executed. Many of these subtasks are named after the task with which they are associated. You may create custom subtasks.

See the help topic Process Framework Overview.

Use the Process Framework Admin Tool to group subtasks and create custom tasks.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?