Feeder Sync Tool
The Feeder Sync Tool enables you to use the functions of Feeder Manager 2.0 while continuing to update the FeederID, FeederID2, and FeederInfo fields after a user has finished editing data interactively. A list of edited features is stored in the MM_EDITED_FEATURES table, allowing the Feeder Manager 1.0 fields to be updated later when a user is not actively using the application. The application can be configured to update the Feeder Manager 1.0 fields when the session is posted with a Geodatabase Manager action handler or by developing a custom feeder sync module. For a developer sample, visit the myArcFM page Synchronize Feeder Information.
|
Table |
Role |
Privileges |
|
MM_EDITED_FEATURES |
MM_ADMIN |
SELECT, INSERT, UPDATE, DELETE |
|
MM_EDITED_FEATURES |
MM_USER |
SELECT, INSERT, UPDATE, DELETE |
Using the Feeder Sync Tool When Posting (Default Configuration)
- In ArcCatalog, right-click your Electric Geometric Network and select Configure Feeder Manager.
- From the Feeder Manager configuration window:
-
Clear the Feeder Manager 1.0 option (if enabled).
-
Select the Feeder Manager 2.0 option.
-
Expand the Advanced Configuration options. Select the Feeder Manager 1.0/Feeder Manager 2.0 Field Sync option.
-
Optionally set the Enable autoupdaters during field sync option to allow autoupdaters to fire during field synchronization.
-
Set the Target version for sync (SDE.DEFAULT by default).

-
- Click OK.
- Create or open a session or design in ArcMap.
- Perform typical editing operations (create/delete features,
editing existing features, etc.) in that session or design.
-
Notice that the Feeder Information fields from Feeder Manager 2.0 update after each edit (Feeder IDs, Subfeeder IDs (if applicable), Energized Phases, Number of Feeders, Loop, Tie Device).
-
Notice that the feeder information in the legacy fields (FeederID, FeederID2, and FeederInfo) do not update after each edit.
-
- Save the session or design. This will populate the MM_EDITED_FEATURES
table.
-
You can add the MM_Edited_Features table to inspect its contents if necessary.
-
- Post the session or design to SDE.DEFAULT. The former Feeder Manager 1.0 fields now populate with the new feeder information (FeederID, FeederID2, and FeederInfo).
Using Feeder Sync with Geodatabase Manager (GDBM)
- Configure the Feeder Sync Tool via the Feeder Manager Configuration window.
- Add the following Action Handlers for the Feeder Sync Tool
to your existing GDBM configuration (see the Tasks topic for more information):
-
Run Feeder Sync assigned to Before Post.
-
Cleanup Feeder Sync assigned to After Post.
-
- Once GDBM has been properly configured for the Feeder Sync Tool, open ArcMap and create a new Session or Design.
- Perform typical editing operations (create/delete features,
editing existing features, etc.) in that session or design.
-
Notice that the Feeder Information fields from Feeder Manager 2.0 update after each edit (Feeder IDs, Subfeeder IDs (if applicable), Energized Phases, Number of Feeders, Loop, Tie Device).
-
Notice that the Feeder Information in the legacy fields (FeederID, FeederID2 and FeederInfo) does not update after each edit.
-
- Save the session or design. This populates the MM_EDITED_FEATURES table. You can add the MM_EDITED_FEATURES table to inspect its contents if necessary.
- Send the Session or Design to the GDBM Post Queue.
- After GDBM runs through the posting process you can inspect the Logging tab for information on the number of features synced and if it was completed successfully.
- Open your SDE.Default version in ArcMap and inspect the legacy FeederID, FeederID2, and FeederInfo fields to see that they have been updated.
ESENT File Cleanup in Geodatabase Manager
Geodatabase Manager deletes all the ESENT files (.edb files) created in AppData\Roaming\Miner and Miner, whenever the Feeder Sync action handler finishes its processing of a version. Microsoft ESENT and Local Storage includes more information on ESENT files.
The cleanup action removes only those files that have reached the age limit configured for Feeder Manager 2's cleanup activity for ESENT files, provided that the files are not still being used by the service. The intent is to prevent the accumulation of a large number of .edb files, rather than ensure the instant removal of every .edb file that appears.