Open Point

You will need to assign the NormalStatus domain to the NormalPosition fields.

  1. Right-click the feature class and select Properties.
  2. Click the Fields tab and select the NormalPosition_A field.
  3. In the Field Properties window, set the Domain field to Normal Status.
  4. Repeat steps 2 and 3 for NormalPosition_B and NormalPosition_C.

    Object Model names: SWITCH

    Field Model names:

    Field

    Field Model Name

    Properties

    FeederID

    FEEDERID

    Field Info Tab:

    Reset After Create = Yes

    FeederID2

    FEEDERID2

    Field Info Tab:

    Reset After Create = Yes

    FeederInfo

    FEEDERINFO

    Field Info Tab:

    Editable = No

    Reset After Create = Yes

    ElectricTraceWeight

    MMELECTRICTRACEWEIGHT

    Field Info Tab:

    Reset After Create = Yes

    PhaseDesignation

    PHASEDESIGNATION

     

    NormalPosition_A

    NORMALPOSITION_A

     

    NormalPosition_B

    NORMALPOSITION_B

     

    NormalPosition_C

    NORMALPOSITION_C

     

    Optional: The following fields are required only if you have a multi-tiered network. The ParentCircuitSourceID field should exist on every feature class that participates in the multi-tiered network. The CircuitSourceID and Subsource fields should be added to all junction classes eligible to represent subsidiary sources.

    ParentCircuitSourceGUID

    PARENTCIRCUITSOURCEGUID

    Field Info Tab:

    Visible = Yes

    Editable = No

    Reset After Create = Yes

    Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

    ParentCircuitSourceID

    PARENTCIRCUITSOURCEID

    Field Info Tab:

    Visible = Yes

    Editable = No

    Reset After Create = Yes

    CircuitSourceGlobalID

    Global ID

    Field Info Tab:

    Visible = Yes

    Editable = No

    Reset After Create = Yes

    CircuitSourceGUID

    GUID

    Field Info Tab:

    Visible = Yes

    Editable = No

    Reset After Create = Yes

    Add either only CircuitSourceID or both CircuitSoureGlobalID and CircuitSourceGUID, but not all three. If all three are added, the feature will not work with the manager.

    CircuitSourceID

    CIRCUITSOURCEID

    Field Info Tab:

    Visible = Yes

    Editable = No

    Reset After Create = Yes

    Subsource

    SUBSOURCE

     Field Info Tab:

    Visible = Yes

    Editable = Yes

    Reset After Create = Yes

    FacilityID

    FACILITYID

    Field Info Tab:

    Reset After Create = No

    Visible = Yes

    Editable = Yes

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?