Close Express Design

Closes an express design that has been opened in ArcMap.

Enabled

  • MMWorkflowManager must be the current extension.

  • The node passed to this subtask is an express design node.

  • Workflow Manager must be open through ArcMap.

  • An express design must be open in ArcMap.

Execute

  1. Prompts the user to save any outstanding edits.

  2. Checks for conflicts.

  3. Reconciles and posts the design.

  4. Closes the express design.

  5. Marks the design's version for deletion (unless it has been opened for as-built editing).

  6. Sets the PxApplication on the Process Framework Tasks tool extension to nothing.

  7. Enables the Stored Items tools.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?