Move Design

Assigns a design to a different work request.

Enabled

  • The selected node must be a design.

  • The design may not be currently open in ArcMap.

Execute

  1. Compiles a list of all available work requests and presents it to the user for selection. This list excludes the selected design’s parent work request and any work requests that have an approved design.

  2. Moves the design to the selected work request.
  3. If the selected design has been approved, the MM_WMS_APPROVED_DESIGNS table is updated.

  4. If moving the design affects the state of the source work request, then there must a valid transition defined that allows the work request state to change before adding the destination work request to the list.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?