Open Edit Session

Opens the session node for editing in ArcMap.

Enabled

  • A session node must be selected.

  • MMSessionManager must be the current extension.

  • You must NOT have an editing session started.

  • Session Manager must be open from ArcMap (not standalone) and visible.

  • User must have access to the appropriate ArcFM Solution license: ArcFM, Designer or Inspector.

  • User must have access to the appropriate Esri license: Engine Geodatabase, ArcGIS for Desktop Standard (formerly ArcEditor) or ArcGIS for Desktop Advanced (formerly ArcInfo).

Execute

  1. Opens the session as editable.

  2. Sets the PxApplication on the Process Framework Task Tool extension.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?