Switches
You will need to assign the NormalStatus domain to the NormalPosition fields.
- Right-click the Switch feature class and select Properties.
- Click the Fields tab and select the NormalPosition_A field.
- In the Field Properties window, set the Domain field to Normal Status.
- Repeat steps 2 and 3 for NormalPosition_B and NormalPosition_C.
Object Model name: SWITCH
Field Model names:
Field
Field Model Name
Properties
FeederID
FEEDERID
Field Info Tab:
Reset After Create = Yes
FeederID2
FEEDERID2
Field Info Tab:
Reset After Create = Yes
FeederInfo
FEEDERINFO
Field Info Tab:
Editable = No
Reset After Create = Yes
GangOperated
FDRMGRGANGOPERATED
ElectricTraceWeight
MMELECTRICTRACEWEIGHT
Field Info Tab:
Reset After Create = Yes
PhaseDesignation
PHASEDESIGNATION
NormalPosition_A
NORMALPOSITION_A
NormalPosition_B
NORMALPOSITION_B
NormalPosition_C
NORMALPOSITION_C
Optional: The following fields are required only if you have a multi-tiered network. The ParentCircuitSourceID field should exist on every feature class that participates in the multi-tiered network. The CircuitSourceID and Subsource fields should be added to all junction classes eligible to represent subsidiary sources.
ParentCircuitSourceGUID
PARENTCIRCUITSOURCEGUID
Field Info Tab:
Visible = Yes
Editable = No
Reset After Create = Yes
Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.
ParentCircuitSourceID
PARENTCIRCUITSOURCEID
Field Info Tab:
Visible = Yes
Editable = No
Reset After Create = Yes
CircuitSourceGlobalID
Global ID
Field Info Tab:
Visible = Yes
Editable = No
Reset After Create = Yes
CircuitSourceGUID
GUID
Field Info Tab:
Visible = Yes
Editable = No
Reset After Create = Yes
Add either only CircuitSourceID or both CircuitSoureGlobalID and CircuitSourceGUID, but not all three. If all three are added, the feature will not work with the manager.
CircuitSourceID
CIRCUITSOURCEID
Field Info Tab:
Reset After Create = Yes
Subsource
SUBSOURCE
Field Info Tab:
Visible = Yes
Editable = Yes
Reset After Create = Yes
FacilityID
FACILITYID
Field Info Tab:
Visible = Yes
Editable = Yes
Reset After Create = No
Things to ensure for correct behavior:
-
Must exist as a simple junction and must split any complex edge
-