Connect to Session Manager on Microsoft SQL Server

If you are using Microsoft SQL Server, the client software is probably installed on your machine already, especially if the machine has ArcFM, ArcGIS, or Microsoft Office installed.

Connecting to a SQL Server database is a simple process. Since the SQL Server Client software can find any SQL Server database servers that are connected to your network, it is sufficient to just specify the server’s host name on your network and the name of the database running on that server.

  1. Determine name of server.
  2. Determine name of the database on the server that hosts the Process Framework and Session Manager tables.
  3. Connect using server name, database name, user name, and password.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?