Configure Duct Bank/Conduit Size Options

To configure Duct Bank/Conduit Size options for use in your geodatabase, follow these steps:

  1. Add the following field model names to the Electric Field Model Name domain.

    DUCTBANKHEIGHT

    DUCTBANKWIDTH

  2. Create the ULS Size and ULS Size Actual domains. The data type of these domains must match the data types of the DuctSize and ActualDuctSize fields (text, float, or double). The ULS Size domain contains coded values that represent the various duct sizes (in map units) available in your underground network. Regardless of data type, the coded values must be numeric, for example, 1.5, 2, 10. The Minerville sample database uses the following domain. You may use the values that apply to your utility.

    Duct Size

    Coded Value

    2"

    2

    5"

    5

    10"

    10

  3. If you use the ActualSize field to maintain the actual size of the duct as well as a relative size that is placed on the map, you will need to create two ULS Size domains. For this example, we created one called ULS Size and assigned it to the DuctSize field. We also created another called ULS Size Actual and assigned it to the ActualSize field.
  4. Add the fields shown below to the Conduit feature class.

    Field Name

    Data Type

    DuctHeight

    text, short or long integer, float or double

    DuctWidth

    text, short or long integer, float or double

  5. Assign the following field model names to the Conductor (Cable) feature classes.

    Field

    Field Model Name

    DuctHeight

    DUCTBANKHEIGHT

    DuctWidth

    DUCTBANKWIDTH

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?