Connect to Session Manager on PostgreSQL

Connecting to a PostgreSQL database is a simple process.

  1. Determine name of server.
  2. Determine name of the database on the server that hosts the Process Framework and Session Manager tables.
  3. Connect using server name, database name, user name, and password.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?