Configure Duct ID Options

To configure the Duct ID option for use in your geodatabase, follow these steps:

  1. Add the following field model name to the Electric Field Model Name domain.

    DUCTID

  2. Create the following field on the DuctDefinition object class.

    Field Name

    Data Type

    DuctID

    String

  3. Assign the following field model name to the appropriate field on the DuctDefinition object class.

    Field

    Field Model Name

    DuctID

    DUCTID

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?