CircuitSourceID Object Class

Optional:

The following object class is required ONLY if you are using a multi-tiered network and Extended Feeder Manager.

CircuitSourceID Object Class

Object Model names: CIRCUITSOURCEID

Field Model names:

Field

Field Model Name

FeederLevel

FEEDERLEVEL

FeederName

FEEDERNAME

ObjectID

CIRCUITSOURCEID

ParentCircuitSourceGUID

PARENTCIRCUITSOURCEGUID

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

PARENTCIRCUITSOURCEID

RelatedFeatureClassName

RELATEDFEATURECLASSNAME

RelatedObjectID

RELATEDOBJECTID

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?