IWA Authentication Only: Edit Services User

If your organization utilizes Portal for ArcGIS for your service and your authentication method is IWA, follow the steps below to correctly set up the logon user for the service.

  1. Open Windows Services Console from Control Panel.

  2. Locate the ArcFM Markup Service entry. This is the name under which the service is installed by default.

  3. Right-click the entry and select Properties.

  4. Click the Log On tab.

  5. Ensure the This account radio button is selected.

  6. Type user/password values for a user who has been configured in Portal to access the markup feature service.

    TIP: This user does not have to be an admin user.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?