Administrating Service Configurations

To delete a feature service configuration from the tenant, you need to navigate to the Mapping plugin on the home screen of Solution Center.

Mapping plugin

On the Operational Maps tab, locate the feature service (or Operational Map) you want to delete from the list and select it. Above the Delete button in the pane on the right side, notice the warning message. Deleting a feature service can cause adverse effects to your maps and apps, for that reason, the app prompts you to confirm delete once you click the Delete button.

TIP: Feature services with sessions still in an open state can’t be deleted.

IMPORTANT: If you have issues accessing feature services from Solution Center and receive the following message, it’s recommended you contact Schneider Electric GIS Support for assistance fixing the issue.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?