Configure Markup to GIS
Configuration of the markup palette is required for Markup to GIS to work properly. The desired ArcFM Mobile operational map should override the default palette on the organization’s markup type with the newly deployed markup palette.
Follow the steps below to configure Markup to GIS.
- In the Editor XI Solution Center plugin, navigate to the Editor Maps tab and select your Operational Map. Then select Markup-to-GIS Schema Mapping on the vertical tab.
- Click the Add
button to display a list of unconfigured markup palettes that can be used to map Markup features to Utility Network features. There may be multiple markup palettes available under a given markup type.
- Select at least one palette URL in the list and click the Create Schema Mappings button to begin the schema mapping process.
- To further modify the configuration to map to UN features,
click the Edit
button. Your view changes to a matrix of combo boxes that contain the domains for the Utility Network.
The left side of the mapping matrix details the schema of the Markup Palette and displays the symbology for Markup layers and Subtype mappings.
The right side of the mapping matrix displays the feature class, asset group, and asset type domains mapped for the Utility Network Operational Map under configuration.
Click the Edit button to change the settings for one of the subtype mappings. The display updates to show drop-downs for each of the feature class, asset group, and asset type domains.
The box drop-downs are populated with feature classes that have compatible Geometry Objects (i.e. Point, Line, Polygon).
Click the Save button once you complete your configuration settings.