Select Your Service Domain Network

When a feature service configuration is successfully created, the form for your new feature service is displayed.

To set the configuration, select the desired Domain Network from the combo box and click the button for your utility type (Electric, Gas, or Water). It is important you select the utility type since different settings are presented in subsequent parts of the form.

Once you have selected the appropriate form, each combo box is filled with the possible fields and settings you can map to for your Utility Network.

IMPORTANT: For your instance of Editor XI to properly work, you must have the below settings configured according to your service domain network type.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?