Workflow Families

Whether in the Default Workflow Studio or the Studio tab, each subtab represents a type of workflow family that corresponds to where the workflows are executed (hosted versus specific client applications such as Editor, Designer, etc.). In the Default Workflow Studio tab, out-of-the-box workflows are provided for each workflow family type. While workflow families have much in common, some have some important distinctions. Continue reading about each type of workflow family to learn more.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?