Logging

The Logging tab provides a time-filtered view of all replica and delta events to assist you with troubleshooting.

This tab provides a full list of logs, in addition to ways of filtering the copious amount of technical information provided. On this tab you can view specific issues according to:

  • Timeframe (#1 in the image above)

  • Minimum level of issue (#2)

  • Advanced filter (#3)

  • Available filters (e.g., Exclude service bus errors, #4)

Once you’ve applied one or more filters, click the Run button on the left. You can also perform a search using the Search field at the top of the app.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?