Conduit Manager

Conduit Manager XI is a set of tools which allows you to maintain the underground infrastructure of your utility network. This set of tools provides the ability to create and manage conduit, underground structures, and duct banks. You can also view the details of your underground structures, such as duct placement and duct configuration.

IMPORTANT: If you have ducts in your map, changing the DuctDiameterUnit and MapUnit settings that your map was initially created with to a different unit of measure is not recommended or supported. Doing so could impact the spacing and size of ducts. It's recommended that once the unit of measure is set, you don't modify it.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?