Markups
When a user taps Submit in the ArcFM Mobile app and receives a message indicating markup sketches have been sent, after a refresh you can see the markup listed in the left pane. In the middle pane, you can view the history of the markup sketch, from the ArcFM Mobile app to the geodatabase, including any potential workflow errors. In the right pane, you can view the markup sketch in the map.
In the left pane, you see a list of all the markup
sketches that have been sent by users in the ArcFM Mobile app. A red exclamation point next to a markup sketch
indicates that it has an associated workflow error. To view only markup
sketches with workflow errors, click the filter with the red exclamation
icon.
You can also sort on markup types by clicking the drop-down icon next to the regular filter and selecting/deselecting types in the list.
After you’ve selected a markup sketch in the left pane, the middle pane shows the markup sketch’s path through assignments. In the case of ad hoc markup sketches in ArcFM Mobile, the path is from field assignment (sketching in the field) to enterprise assignment (viewing the sketch on the desktop).
If the markup sketch is active and hasn’t made it to enterprise assignment, then in the right pane you see a preview in ArcGIS of the markup sketch.
If
the expected markups do not reside in the map, we recommend that you
click the Refresh button at the top of the
middle Markups pane.