Gas Device and Pipeline Summaries Configuration

The following keys must be configured in Editor XI configuration to show device information correctly:

Key Name

Description

Default Value

Gas Facility Id

Field in which the title of the Component Info pane will show after a device is selected, e.g. ASSETID.

ASSETID

Gas Design Type

This key must be mapped to the field with proper domains related to the type of valve (e.g. Ball, Butterfly) and is represented by Valve Type in Component Info.

DESIGNTYPE

Gas Device Material

This key must be mapped to the field with proper domains related to the type of material the device feature is made from (e.g. Cast Iron, Steel) and is represented by Material in Component Info.

MATERIAL

Gas Device Diameter

This key must be mapped to the field with proper domains related to the diameter of features in the map and is represented by Diameter in Component Info.

TIP: Changing the units in the Editor XI Configuration does not change the units of the diameter field.

DIAMETER

Gas Device Critical

This key must be mapped to the text field which contains information about the operating classification of the valve (e.g. Critical). It is represented by Critical in Component Info.

IMPORTANT: While Component Info indicates Yes or No, the User Interface is searching for the string ‘cr’ in upper or lower case within the attribute of the valve feature. To denote that a valve is not critical do not use any words with ‘cr.’

IMPORTANCE

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?