Water Domain

Water Settings

Water General Settings

Settings

WaterDistributionTierName

System

Water Field Names

The Field Model Names listed below are given in Solution Center, and they are then pointed to user-selected Database Fields.

The Database Field Name list below matches Schneider Electric sample data, however, it is not required that your data matches these exactly. The Field Names can be called anything you desire. However it is required that the Field Model Names match as indicated in the table below.

TIP: If your organization chooses to name your database fields differently than those listed below in the column below, it is recommended that you record what database names you assigned to which field model names in place of the suggested names in the table. This list of differences will help assist Schneider Electric Support in the event you need their assistance with your database in the future.

Field Model Name

Database Field Name

Device Status

presentstatus

FacilityId

assetid

PipeDiameter

diameter

Water Class Model Names

Class Model Names don't have to match exactly as illustrated in the table below. You can set any of your features with the Water Device model name as long it is a Controllable Device within Component Info.

Feature Class

Asset Group

Asset Type

Water Device

Controllable Valve

<All Types>

The Class Model Names tab of the feature service is the Model Name Manager. These model names are applied directly to a selection of asset types, or to all asset groups.

Model Name

Assign To:

GasValve

Assign this model name to valve asset types to enable Component Info functionality for the asset.

WaterValve

Assign this model name to valve asset types to enable Component Info functionality for the asset.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?