Gas Domain

Gas Settings

Gas General Settings

Settings

GasDistributionTierName

Pipe Distribution System

PipeDiameterUnits

Centimeters

Gas Field Names

The Field Model Names listed below are given in Solution Center, and they are then pointed to user-selected Database Fields.

The Database Field Name list below matches Schneider Electric sample data, however, it is not required that your data matches these exactly. The Field Names can be called anything you desire. However it is required that the Field Model Names match as indicated in the table below.

TIP: If your organization chooses to name your database fields differently than those listed below in the column below, it is recommended that you record what database names you assigned to which field model names in place of the suggested names in the table. This list of differences will help assist Schneider Electric Support in the event you need their assistance with your database in the future.

Field Model Name

Database Field Name

DeviceAssetTypeNetworkAttribute

G_DEVICEASSETTYPE

DeviceCritical

importance

DeviceDiameter

diameter

DeviceMaterial

material

DeviceStatus

devicestatus

DeviceType

designtype

FacilityId

assetid

Pinchable

pinchable

PipeDiameter

nominaldiameter

StructureFacilityId

assetid

Gas Class Model Names

Class Model Names don't have to match exactly as illustrated in the table below. You can set any of your features with the Gas Device model name as long it is a Controllable Device within Component Info.

Feature Class

Asset Group

Asset Type

Gas Device

Controllable Tee

Controllable Tee

Gas Device

Controllable Valve

System

Gas Device

Regulator

Regulator

Gas Device

Controllable Valve

Emergency

Gas Device

Meter

Custody Transfer

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?