Conduit Manager Data Model

Use this section to make sure your data model is accurately set up to properly run Conduit Manager. The data model is broken in to Domains, Subtypes, Fields, and Rules for easier navigation and viewing of the model.

IMPORTANT: The Conduit Manager data model is flexible allowing Administrators to use different terms within their data model as compared to the examples provided in this section. For example, instead of calling it a duct, your organization may prefer to call it conduit or tube. Swapping out one term for another is allowed, however, it is strongly encouraged you keep the term consistent throughout the data model.

It’s highly recommended you look through the entire Conduit Manager data model before beginning to configure Conduit Manager to look for areas where you would prefer to use a different term so the same terms can be used throughout the entire data model.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?