Markup

Markup tools allow users to place graphics in the map in ArcFM Mobile and send them off to a GIS analyst who uses Editor XI to make permanent changes in the database.

Take it for a drive!

(The link opens/switches to the Solution Center app and accesses the Markup plugin.)

The Markup plugin lists every markup sketch (and its related assignments) that users have submitted, and provides you with tools and error logs to help diagnose any problems that may arise with them successfully sending markups back to the geodatabase. You can define as many Markup Types as you need, define default palettes, and view service settings. The plugin has tabs for Markup Types, Markups, and Logs. This section contains detailed explanations of each tab.

Markups tab

As with all other available plugins, you can install the Markup plugin via Plugins on the main Solution Center window.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?