ArcFM UN Compatibility Status

Under Editor Settings in the Editor Maps tab, you can also check the check compatibility status of new electric data set configurations through the ArcFM UN compatibility status tool.

Click the Verify ArcFM UN compatibility button to run the status check.

When the check completes, either a check mark or an exclamation point displays next to the text. A check mark indicates the UN is compatible. An exclamation point indicates there are invalid network categories.

Click on the Notifications button in the top right of the Solution Center window to display the notifications list. This list contains a separate notification for each invalid network category.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?