ArcFM Connectivity Evaluator (ACE)

The ArcFM Connectivity Evaluator (ACE) is a separate application from Solution Center. Its core function is to test and verify connectivity to ArcFM services and, depending on the application, connectivity to Azure Service Bus. This is a crucial prerequisite prior to performing Solution Center configuration or any XI series app configuration, given that you need connectivity for the configuration to work.

IMPORTANT: Schneider Electric is continuously making changes to increase the reliability and resilience of our services. Our development teams have introduced features that allow automatic failover services for all primary services. We are leveraging Azure features called Application Gateway and Traffic Manager to enable every customer to have a primary and secondary region. This requires a minor change to firewall rules on your side plus coordination with our Operations team. To read more about this change, refer tp the App Gateway article on myArcFM.

Access the ACE Installer

The ACE installer can be downloaded via the ArcFM Solution Center article on myArcFM.

Because the ACE tool is testing connectivity, it only works after your company’s tenant is created.

IMPORTANT: If you are having basic connectivity issues, you might need to allowlist the tenancy service itself: https://tenancy.arcfmsolution.com.

The ACE tool can be run as many times as needed until all issues are corrected. This is particularly true throughout the implementation process.


Verify Core Outbound URL Access

Verifying access to the core outbound URLs is extremely helpful during the very early stages of your implementation. This verification includes the ability to access core ArcFM Services, Auth0, and the Tenancy service itself. Access to these core services is a prerequisite for essentially any other configuration or implementation step.

To verify access, follow these steps:

  1. Launch the ACE tool.

    IMPORTANT: Verifying core outbound URL access can happen on any machine. The ACE tool does not necessarily need to be installed on the same machine that contains the actual XI series application. To check core outbound URLs, you only need the ACE tool and tenant ID. To verify access to other services and the Azure Service Bus, the ACE tool needs to be installed on the same machine as the actual application.

  2. If this is the first time you have launched the tool, “Please enter your organization’s name” then click Submit.

  3. You don’t need to log in to check core outbound URLs. Refer to the Firewall Rules for Ports topic for more information.

  4. Click the View <tenantName> Allowlist button.

  5. The interface displays icons for All Services and for Login Info.

    1. To see all the required URLs for all services, click All Services.

    2. Click Open Services Report to generate a PDF of service URLs. This is a great way to share the URLs that require allowlisting.

    3. To test access to the actual URLs, click the desired service icon (for example, the Login Info icon).

      1. You can test services individually, or click the Test All icon to start the process (the URLs in the following image are just examples and your URLs differ). When you click All Services, you are provided with a full application allowlist, similar to the following image:


        When you click Login Info, you are provided with a way to test all services that are required to log in. The tests need to be initiated on the machine that hosts any ArcFM XI series application.


        After running a test, the application displays the test results along with an HTTP status code.

        The following table includes a description of the possible result codes, whose standard descriptions are taken from the protocols established by the Internet Engineering Task Force (IETF):

        Code

        Result

        Description

        Troubleshooting

        200

        OK

        The request has succeeded. The information returned with the response is dependent on the method used in the request

        The server responded as expected.  The service is functioning normally.

        302

        Found

        The requested resource resides temporarily under a different Uniform Resource Identifier (URI). Since the redirection might be altered on occasion, the client should continue to use the Request-URI for future requests. This response is only cacheable if indicated by a Cache-Control or Expires header field.

        Most likely a misconfigured service URL.  Copy test results, contact support, and include copy of test results.

        400

        Bad Request

        The request could not be understood by the server due to malformed syntax. The client should not repeat the request without modifications.

        Problem with the ACE tool. Update to current version and try again.

        401

        Unauthorized

        The request requires user authentication.

        Problem with ACE tool not sending an appropriate authentication header.  Update to current version and try again.

        403

        Forbidden

        The server understood the request, but it is refusing to fulfill it.

        Misconfigured service permissions.  Make note of the service being tested.  Copy test results, contact support, and include copy of test results.

        404

        Not Found

        The server has not found anything matching the Request-URI. No indication is given of whether the condition is temporary or permanent.

        Misconfigured service endpoint.  The service has been removed, is down, or customer has not been configured for service. Copy test results, contact support, and include copy of test results.

        407

        Proxy Authentication Required

        Indicates that the client must first authenticate itself with the proxy.

        Customer has proxy in use and user must authenticate to proxy first before connecting to ArcFM services.  Copy test results, contact support, and include copy of test results.

        408

        Request Timeout

        The client did not produce a request within the time that the server was prepared to wait. The client may repeat the request without modifications at any later time.

        Several possible causes: non-existent endpoint, customer proxy did not forward request to ArcFM services, etc. If error repeats upon re-try at a later time, copy test results, contact support, and include copy of test results.

        500

        Internal Server Error

        The server encountered an unexpected condition which prevented it from fulfilling the request.

        Problem with ArcFM service endpoint.  Update to current version and try again. If error repeats, copy test results, contact support, and include copy of test results.

        502

        Bad Gateway

        The server, while acting as a gateway or proxy, received an invalid response from the upstream server it accessed in attempting to fulfill the request.

        Most likely caused by customer firewall or proxy.  Could be a single endpoint or all.  If a single endpoint, add the service endpoint URL to the firewall and/or proxy and try again.  If error repeats, copy test results, contact support, and include copy of test results.

      2. Optionally, click Open Test Report to generate a PDF version of the test results.

        NOTE: Reports are saved in the directory C:\Users\user_name\AppData\Local\ArcFMConnectivityEvaluator\app-version#\Reports.


Verify Application-Specific Services and Connectivity to Azure Service Bus

Going a step further, after verifying core services, it is also critical to verify access to application-specific services and to the Azure Service Bus. Each XI Series application provides details of the required connections and ports, and the ability to test the connections in bulk or individually. The ACE tool handles both core and application-specific services, but the key difference is in order to check application-specific services, the ACE needs to be installed on the same machine hosting the app itself.

  1. If necessary, download and install the ACE tool on the same machine that runs the XI application you are testing. In other words, if you are testing connectivity for Designer XI, run the tool on the same machine where Designer XI is installed.

  2. Launch the ACE tool and log in to your tenant.

  3. If your users have access to multiple tenants, they can switch between them using the tenant drop-down list.

  4. The interface displays icon for the various, application-specific services in addition to All Services.

  5. As explained previously, All Services provides a view-only list of URLs.

  6. Test connectivity to a service by clicking the desired service icon (for example, the Solution Center icon), then click the Test All icon to test access.

  7. Optionally, click “Open Test Report” to generate a PDF version of the test results.

Authenticate with the ACE Tool

In the event that you need to use the ACE tool for authentication, within the app select the appropriate tenant from the drop-down list.

After selecting a tenant and successfully authenticating, you can view the full application allowlist.


The ACE tool window provides two options: All Services and Login Info.


When you click All Services, you are provided with a full application allowlist, similar to the following image:


When you click Login Info, you are provided with a way to test all services that are required to log in. The tests need to be initiated on the machine that hosts any ArcFM XI series application.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?