Session Display Filters

The Session Manager sessions list can be filtered to show sessions with a certain status for a smaller session list to look through. This functionality is available in both Editor XI and Solution Center.

Click the Filter list of sessions by status button to display the list of possible filters.

By default all toggles are turned on, indicated by a green and white toggle switch. Click the toggles to turn off the status types you don’t want to see listed. Turn the toggle back on by clicking it again. You can also use the Select All or Unselect All buttons to turn on or off all the toggles at once.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?