Test Proxy

After establishing your Hybrid Connections and uploading your certificates, the Test Proxy tab allows you to test your configurations. It ensures the application can communicate with the services and that the services can communicate back. This is particularly helpful if you are setting up a new Portal or a new ArcGIS Server.


Follow these steps to execute a test:

  1. In the URL field, choose the service to test.

    • This drop-down is pre-populated with the URLs from the Portal Login Configuration tab.

    • You can paste in other URLs to test.

  2. Click Execute.

  3. Read through the Result Codes and, if applicable, the Error Message to help troubleshoot issues.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?