Electric Domain
Electric Settings
Electric General Settings |
Settings |
---|---|
ElectricDistributionTierName |
Electric Distribution |
TransformerAttachRadiusInMapUnits |
Enter a value, likely between 0.20 and 50.00. A structure found within this radius (with rules that allow attachment) is automatically considered as attached to the given device when performing an in-line network feature or transformer move. |
TransformerToLineRadiusInMapUnits |
Enter a value, likely between 0.20 and 50.00. This value is the default offset distance from the connection point and transformer during a transformer move. |
TrimAndConnectRadiusInMapUnits |
Enter a value between 0.20 and 50.00. This value is the distance, in map units, that separates the line-ends from the placed device when using the Trim and Connect tool. |
Electric Field Names
The Field Model Names listed below are given in Solution Center, and they are then pointed to user-selected Database Fields.
The Database Field Name list below matches Schneider Electric sample data, however, it is not required that your data matches these exactly. The Field Names can be called anything you desire. However it is required that the Field Model Names match as indicated in the table below.
Field Model Name |
Feature Class |
Database Field Name |
Data Type |
Description |
---|---|---|---|---|
ConductorMaterial |
ElectricLine ElectricEdgeObject |
conductormaterial |
Short |
Integer code for conductor material. |
ConductorOperatingVoltage |
ElectricLine ElectricEdgeObject |
voltagegroup |
Short or Long |
Integer code for the nominal operating voltage (values should include units and indicate whether the value is line-to-line or line-to-neutral). Examples:
|
ConductorSize |
ElectricLine ElectricEdgeObject |
conductorsize |
Short |
Integer code for conductor size. |
CustomerLoad |
ElectricSubnetline |
customerLoad |
Short or Long |
Designates a numeric field whose value is assigned by a subnetwork summary function that computes the sum of service panel amp ratings for all service points on the subnetwork. Used by Network Management in Editor XI to produce an estimate of feeder load MVA. |
DeviceStatus |
ElectricDevice ElectricJunctionObject |
devicestatus |
Short |
Values: Open, Closed |
ElectricSubnetworkName |
ElectricLine ElectricDevice ElectricEdgeObject ElectricJunctionObject |
subnetworkname |
Text |
Field to which the UpdateSubnetwork function writes the subnetwork name for a feature. |
FacilityId |
ElectricLine ElectricDevice ElectricEdgeObject ElectricJunctionObject |
assetId |
Text |
Identifier preferred by the organization implementing ArcFM. |
FuseRatedAmps |
ElectricDevice ElectricJunctionObject |
devicesize |
Short |
Integer code for the fuse rating. |
IsGangOperated |
ElectricDevice ElectricJunctionObject |
gangoperated |
Short |
Indicates if the device controls all phases together. |
PhasesCurrent |
ElectricLine ElectricDevice ElectricEdgeObject ElectricJunctionObject |
phasesnormal |
Short |
Represents the phases present for each device. |
PhasesCurrentNetworkAttribute |
ElectricLine ElectricDevice ElectricEdgeObject ElectricJunctionObject |
E:Phases Normal |
N/A — network attribute, not a field. |
An in-line network attribute associated with the PhasesCurrent field. |
RatedKva |
ElectricDevice ElectricJunctionObject |
devicesize |
Double |
Integer code for the power rating of a device (e.g. transformer rated power). |
StructureFacilityId |
Structure Boundary |
assetId |
Text |
Identifier preferred by the organization implementing ArcFM, for structural facilities. |
Electric Class Model Names (Network Categories)
In Editor XI, electric class model names have been replaced with network categories. For network category configuration, see Appendix A in the ArcFM Configuration for the Utility Network white paper in myArcFM.