Logs

The Logs tab provides ways for you to search various durations of logs, types of logs, applications for which you have licenses, connections configured for applicable services, and any additional queries that you can specify.

  1. Duration: select a timeframe in which to search, from the last 30 minutes up to the last 90 days.

  2. Log Types: select the type of logs to search, from errors to push notifications.

  3. Application: select the application to search for which you have organizational licenses.

  4. Connections: select the type of connection to search, from a list of configured connections.

  5. Additional Query: type additional search criteria using the examples provided in the drop-down.

  6. Load More: loads more results not currently visible in the results field.

  7. Jump to Top/Jump to Bottom: takes you to the top of the results field or the bottom, respectively.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?