Utility Network Configuration
Solution Center automatically installs the Editor XI plugin according to your licenses. However, your organization needs to complete additional configuration to properly work with your data.
To complete the necessary configuration, you need to start on the Editor XI Maps tab in Solution Center for Editor. You might also have to select your utility domain from the Select a Domain Network to configure drop-down.
On the Class
Model Names vertical tab, click the Add New button to add additional class model names as outlined for your
domain network.
The Undo button is visible when you are updating
mapped fields and settings but the updates haven’t been saved
yet. Click this button to undo changes made after the most recent
save.
Model name configurations are deleted by clicking the
Delete button next to the model name setting on the Class Model
Names tab.
Follow the instructions in this section to configure the Editor XI plugin for your utility domain.