Unassign Session

Sessions can be unassigned in the Session Manager tab of Solution Center. Unassigning a session puts the session back in the queue of available work within Session Manager. Follow the steps below to unassign a session.

  1. In Solution Center > Editor > Session Manager, find the desired session.

    TIP: Type the session name into the Search field at the top of the interface to quickly find your session.
  2. Click the Assignments Tab.

  3. Click Reassign.

  4. In the Assign To dialog, click “Available Work - Unassign.”

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?