Editor Client Workflows
The Editor Client subtab, or workflow family, of the Default Workflow Studio is the home of client-side workflows specific to the Editor XI application. Some examples are the Create Session, Open Session, and Delete Session workflows. Think of these client-side workflows as actions an individual might take on their individual computer while working with the application.
Available Tools
The functions, tools, and subtabs are largely the same between the Studio and Default Workflow Studio tabs. However, the Studio tab provides a few additional tools on its subtabs.
The following buttons are available on all subtabs in Default Workflow Studio. Refer to the Studio topic to learn about its additional tools.
Revision history of a workflow is recorded and can be helpful to track changes made to different versions of workflows over time. Refer to the Default Workflow Studio topic to read more about revision history records.
Below is an example of an Editor Client workflow, the Create Session workflow.
Workflow Properties
Property | Definition |
---|---|
Name |
The title of your workflow. |
Minimum Client Version |
The minimum version of Editor required to execute this autoupdater workflow. This field only applies to autoupdater workflows on the ArcGIS Server subtab. We recommend leaving this field blank on all other types of workflows. |
Workflow Status |
Published — the workflow is published and represents the latest version of the workflow. Draft — the workflow is in draft form and not published. Retired — the workflow has been replaced by a newer version and this version is retired and no longer published. Example — this is a workflow example that is useful for copying and pasting into a new workflow as a template or starting point. |
Workflow Metadata Id |
The unique identifier on each version of a workflow that allows you to call a particular version. |
Workflow Ancestral Id |
This identifier designates the starting point of a workflow’s history, after which all versions maintain that Ancestral Id. |
Version |
The version number of the workflow. Useful in tracking the evolution of workflows as administrators make changes. |
Updated By |
The user name of the last person to modify the workflow. The OOTB workflows provided by Schneider Electric say Updated By Schneider Electric Team, or sometimes say none. |
Updated On |
The date the last workflow modifications were made. |
Expression Language |
The coding language that is used within the workflow. |