Messaging

Messaging displays dead letter messages that exist in the service bus, which helps determine tasks or operations that have failed within an application. This information also helps you track down and debug a failed task. You can also resubmit or delete a specific message.


Click here to take it for a test drive.

This opens Solution Center straight to the Messaging tab.


There are two tabs within Messaging: Topics and Queues.

  • Topics include messages surrounding a number of services that call upon the same event.

  • Queues include messages surrounding services that call upon a series of structured events called a queue.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?