BQT6904800 -03

Treatment of Firmly Screw-Connected Contact Surfaces

WARNING
HAZARD OF INAPPROPRIATE ASSEMBLY
  • When handling bars insulated by heat-shrinkable sleeves, ensure that heat-shrinkable sleeve does not get in contact with lubricant to prevent swelling.
  • Do not touch the contact areas coated with lubricant Mobilith SHC 100.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Follow the below steps for treatment of firmly screw-connected contact surfaces:

  1. Before screw fastening, contact areas must be subjected to preliminary treatment.

Table 21 Pre-treatment for the Material of Contact Surfaces

Material of contact surfaces

Pre-treatment

Silver-plated contact surfaces

Clean(1)

Hot-galvanized sheet-metal

Clean(1), passivation need not be removed

Copper or copper alloy

Clean(1),

expose metallic surface(2)

Aluminium

Clean(1),

expose metallic surface(2)

Steel

Clean(1),

expose metallic surface(2)

Zinc-plated steel

Remove passivation, not the zinc layer(3)

Nickel-plated contact surfaces

Remove passivation layer(4)

(1) Clean by means of lint-free cloth; use cleaning agent in case of serious contam-ination.

(2) Expose metallic surface

  • by treating the entire surface with emery cloth or a rotating grinding tool (grain-size 100 or 80) or

  • using a wire brush which is clearly marked for use exclusively for aluminium or exclusively for copper.

(3) Using a brass brush, steel brush.

(4) Rub slightly by hand using Scotchbrite abrasive agent (Ni layer must not be reduced).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?