BQT6904800 -03

E/S Keylock in OFF Position

Initial Situations:

Check the key is available in the key slot, and make sure it is in the unlock position.

NOTE: The slider can be moved up and down, when the key is in the unlock position.

  1. Lift the slider up and block the access to insert the E/S handle.

  2. Turn the key clockwise to the lock position.

  3. Check the lock open flap slides out and engages with slider.

    • The slider can not be move down to block the access to E/S handle insertion.

    • Remove the key from the key slot.

    Figure 37
    E/S Handle Insertion in OFF Position

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?