BQT6904800 -03

Rating Plate

The type designation on the rating plate specifies the technical data for the cubicles. Refer to Figure 7.

To access this information, flash the QR code with smartphone or connected tablet. This will direct to the website containing the data relating to the device.

When submitting enquiries to the manufacturer or ordering spare parts, the following information is required:

  • Type designation

  • Job number

Figure 7
Components of Rating Plate

1

Type designation

3

Job number

2

Technical data

4

QR code with product information

NOTE: The images shown here are for illustration purpose only.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?