BQT6904800 -03

Switching a Feeder

Initial Situation:

  • VCB: OFF

  • EvoPacT HVX VCB truck: In disconnected/test position

  • E/S: OFF


Switch Feeder Cable ON

Follow the below steps to switch feeder cable ON:

  1. Move truck the into connected/service position (1).

  2. Switch ON the VCB (2).

Figure 49
Switch Feeder Cable ON


Switch Feeder Cable OFF

Follow the below steps to switch feeder cable OFF:

  1. Switch OFF the VCB.

  2. Move truck the into disconnected/test position.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?