BQT6904800 -03

Auxiliary Products

WARNING
HAZARD OF INAPPROPRIATE OPERATION
Comply with the manufacturer safety data sheets for the auxiliary products.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Table 13 Auxiliary Products

Auxiliary product

Order number

Cleaning agent

S008152

Lubricant KL, 0.5 kg can

ST312-111-835

Liquid lubricant FL, 0.5 kg can

S008153

Repair paint, 500 g can, RAL9003, silk-grey

S009 492

NOTE: The auxiliary products are provided by the manufacturer. The use of alternative auxiliary products is not permissible.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?