BQT6904800 -03

Access to the Cable Compartment

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Before accessing the cable compartment, ensure the following:
  • E/S is ON.
  • EvoPacT HVX VCB is OFF and in disconnected/test condition.
  • Check the VDIS indication for zero voltage across the cubicle.
Failure to follow these instructions will result in death or serious injury.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?