BQT6904800 -03

EvoPacT HVX VCB

Figure 12
EvoPacT HVX VCB

1

Main front cover

9

Keys

2

LV Connector (cubicle side)

10

Access to spring charge

3

LV Connector (breaker side)

11

Handle

4

Switch OFF push button

12

Label for EvoPacT HVX VCB operating instructions

5

Switch ON push button

13

Rating plate

6

Operation counter

14

Removable top cover

7

Spring charged and ready-to-close indicator

15

Power connections

8

Main contact position indicator

   
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?