BQT6904800 -03

Switching OFF the E/S

Follow the below steps to switch OFF the E/S:

  1. Press the slider (2) downwards until access to the E/S operation is available.

  2. Insert E/S handle (1) aligned with axis point.

  3. Turn the E/S handle (1) counter-clockwise by 180°.

  4. Check the E/S position indicator through cable compartment inspection window and make sure that the E/S is OFF.

  5. Remove the E/S handle (1) and place it back into the transport trolley.

Figure 46
Switching E/S OFF

1

Handle

2

Slider

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?