BQT6904800 -03

E/S Keylock in ON Position

Follow the below steps to block the access to E/S handle insertion:
  1. Check the key (1) is inserted in the key slot.

  2. Turn the key (1) clockwise to the lock position.

  3. Check the lock close flap (2) slides out and blocks the access to insert the
    E/S handle.

  4. Remove the key (1) from the key slot.

    NOTE: The key (1) can be removed only in the locked position.

    Figure 38
    E/S Handle Insertion in ON Position

    1

    Keylock 1

    2

    Lock close flap

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?