BQT6904800 -03

Earthing the Busbar

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Trucks (EvoPacT HVX VCB and EvoPact MTX) in the appropriate busbar sections must be in the disconnected position.
  • Observe the conditions of Operations and Interlocks.
Failure to follow these instructions will result in death or serious injury.

Earthing the Busbar with Busbar E/S in the Metering Panel

Initial situation:

  • E/S : OFF

  • Metering truck EvoPact MTX: in service position

Earthing the busbar

Switch ON the E/S (1).

Figure 52
Earthing the Busbar with Busbar E/S in the Metering Panel

De-earthing

Switch OFF the E/S.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?