BQT6904800 -03

Switching the VCB Electrically

Switching ON (Closing)

Actuate closing release via bay computer or remote control.

The energy storing device can be charged immediately after switching ON (either by hand or by motor). If voltage is applied to the motor, charging is performed automatically.

Switching OFF (Opening)

  • Actuate the opening release via the bay computer or the remote control

  • By undervoltage release or

  • By secondary release

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?