BQT6904800 -03

Removal and Insertion of LV Connector

The LV connector can only be removed or inserted while the truck is in its disconnected/test position.

Removal of LV Connector

  1. Pull the interlocking lever of the LV connector forward and remove the connector.

  2. Fix the LV connector to the pin on the EvoPacT HVX VCB.

Figure 69
LV Connector EvoPacT HVX VCB

Insertion of LV Connector

  1. Remove the LV connector from the fixation pin on the EvoPacT HVX VCB Refer to Figure 69.

  2. Insert the LV connector into the socket of interchangeability interlock inside the cubicle above the EvoPacT HVX VCB (2).

Figure 70
LV Connector Inside the Cubicle

1

LV Connector

2

EvoPacT HVX VCB

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?