BQT6904800 -03

Electromagnetic Interlocks (Optional)

WARNING
HAZARD OF INAPPROPRIATE OPERATION
Ensure that the switchgear interlocking is complete.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Electromagnetic blocking coils can be used for inter-panel as well as intra-panel interlocks:

  • The EvoPacT HVX VCB ON and OFF pushbuttons are blocked.

  • Manual actuation of the E/S is blocked.

NOTE:
  • In case of failure of the supply voltage, all electrical interlocks are in the locked position. Measure: Re-establish supply voltage.

  • Note the purchase contract and the switchgear specific circuit diagram as regards the design of the interlocking systematics.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?